Part Number: MSP432E401Y
Hi, I was wondering how I can pass an argument to my UART ISR
I would like to access the object coordinator but I cant seem to unless I construct the object outside of my main loop
extern "C" void UART0_IRQHandler(void)
{
uint32_t ui32StatusA;
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32StatusA = UARTIntStatus(UART0_BASE, true);
ui32Status = UARTIntStatus(UART0_BASE, true);
if((ui32StatusA & UART_INT_RX) == UART_INT_RX){
char byte = UARTCharGetNonBlocking(UART0_BASE);
coordinator.modemManager.buffer.push(byte);
UARTIntClear(UART0_BASE, UART_INT_RX);
}
else if((ui32Status & UART_INT_TX) == UART_INT_TX){
coordinator.modemManager.sendNextByte();
UARTIntClear(UART0_BASE, UART_INT_TX);
}
}