Part Number: TMS570LS0332
Tool/software: Code Composer Studio
We are using our functions to check flash CRC.
Also, we have enabled the ECC core for check ECC erros in flash.
The issue: We have a abort exception error: ATCM ECC Error if the Size input the CRC function have this value 0x0001F800U.
The function start checking at the address: 0x00000000.
This error is not triggered if we change the size value. Right now, it is 0x00012C00U.
Thanks