Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: Power up sequence

Part Number: MSP432E401Y

Hello

 

I have some question for power up sequence of MSP432E401Y.

1)
The datasheet says that VDDA have to be powered on before VDD if VDDA and VDD are separated.
I want to confirm this requirement. Is it OK if VDDA-VDD >= 0V is kept like the below figure during all power up period?

 

2)
While both max values of t_VDDA_RISE and t_VDD_RISE are defined as infinite, t_VDDC_RISE is defined as MIN=10usec and MAX=150usec.
But VDDC is generated by the internal LDO. If t_VDD_RISE is less than 10usec or over 150usec, t_VDDC_RISE can’t be within 10usec-150usec.
I think the t_VDDC_RISE requirement contradicts the t_VDD_RISE requirement.
What does it mean?

 

Regards,
Oba