Part Number: TIDM-TM4C129POEAUDIO
Other Parts Discussed in Thread: TIDM-TM4C129POE
Hello?
I have three TIDM-TM4C129POE modules.
I am testing by connecting an audio output(eg mp3) to the input of each module
and connecting an amplifier to each output.
The connection (CALL-RECEIVE) works well.
However, after operating normally for several seconds, several minutes,
or several hours, one module stops (system down).
Only one module is stopped. Stopped modules do nothing.
No audio output, no LED blinking, no touch screen input, etc. all do not work.
Version of program and source file in use:
TivaWare_C_Series-2.2.0.295
CCS version 6/9/10
opus version 1.1.2 / 1.1.5 / 1.2.1 / 1.3.1
Even if all CCS versions and all opus versions are combined and compiled, the result is the same.
The same goes for testing by changing modules.
It is being used without modifying the contents of the source file.
I don't know what the problem is.