This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6638K2K : Question about ip fragmentation

Other Parts Discussed in Thread: TCI6638K2K

Hi,
We have a problem with IP fragmentation. We have two TCI 6638K2K cards.
We do IP fragmentation with the same code for both cards. We see that the packages with ip fragmentation are transmitted to the next hardware on first card. The SoC revision of first card is 3.1. However, we see that the packages with ip fragmentation are not transmitted from PA to the next hardware on second card. The SoC revision of second card is 2.0.
What can be the problem? Could there be a problem caused by revision?
Thanks.