This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: HOW TO POST DATA TO WEBPAGE

Part Number: MSP432E401Y


Dear TI Members,

I am working on the sdk example,"httpserver_MSP_EXP432E401Y_tirtos_ccs". In my application i would like to GET AND POST some parameters like baud rate, data bits from html web page.

I have developed a sample web page "index.html" and  for that i have generated "index.h" file by using "makefsfile.exe".

And i am calling the "index.html" web page in "URLSimple_process" using URLHandler_GET method and 

HTTPServer_sendSimpleResponse(ssock, returnCode, contentType,INDEX_SIZE,index) function.

So after downloading the code, i have opened corresponding html page using: ip_address/index.html. and it was successfully opening the web page.

Now, i would like to know how to retrieve the data using URLHandler_POST method and also what are the changes i need to do in html page and in URLSimple_process function.

html file: 

<html>
<head>
<title> PORT SETTINGS </title>
<head>

<body>
<div id="heading">
<table width="100%">
</div>


Serial Parameters<br />

BaudRate: <select name = "BaudRate">
<option>4800
<option selected>9600
</select> <br>

Data bits: <select name = "Data bits">
<option>7
<option selected>8
</select> <br>

<br/>
</div>


<input type="submit" value="Submit" name="submit" />

</table>
</div>
</body>

</html>

 

URLSimple_process Function:

int URLSimple_process(URLHandler_Handle urlHandler, int method,
const char * url, const char * urlArgs,
int contentLength, int ssock)
{
int status = URLHandler_ENOTHANDLED;
char *body = NULL; /* Body of HTTP response in process */
char *contentType = "text/html"; /* default is "text/plain", but can be overridden */
char *retString = NULL; /* String retrieved from server */
char *inputKey = NULL; /* Name of value to store in server */
char *inputValue = NULL; /* Value to store in server */
char argsToParse[MAX_DB_ENTRY_LEN];
int returnCode; /* HTTP response status code */
int retc; /* Error checking for internal funcs */

/* Determine the corresponding URL on the server */

if (strcmp(url, "/index.html") == 0)
{
if (method == URLHandler_GET)
{
body = "/get 'login.html': This is the login page.";
returnCode = HTTP_SC_OK;
status = URLHandler_EHANDLED;
HTTPServer_sendSimpleResponse(ssock, returnCode, contentType,
INDEX_SIZE, INDEX);
}
else if (method == URLHandler_POST)
{
inputValue = strtok(NULL, "=");
retc = serverPost(inputKey, inputValue);
if (retc == ERR_BAD_INPUT)
{
body = "Failed to POST. The data string is invalid.";
returnCode = HTTP_SC_BAD_REQUEST;
status = URLHandler_EERRORHANDLED;
}
else if (retc == ERR_DB_FULL)
{
body = "Database is full";
returnCode = HTTP_SC_SERVICE_UNAVAILABLE;
status = URLHandler_EERRORHANDLED;
}
else
{
body = "Data string successfully posted to server.";
returnCode = HTTP_SC_OK;
status = URLHandler_EHANDLED;
}
}
}

else if(method == URLHandler_PATCH)
{
body = "PATCH is not handled by any handlers on this server.";
returnCode = HTTP_SC_METHOD_NOT_ALLOWED;
status = URLHandler_ENOTHANDLED;
}
else if(method == URLHandler_DELETE)
{
body = "DELETE is not handled by any handlers on this server.";
returnCode = HTTP_SC_METHOD_NOT_ALLOWED;
status = URLHandler_EERRORHANDLED;
}

if (status != URLHandler_ENOTHANDLED)
{
if (contentLength > 0)
{
char *buf;

buf = malloc(contentLength);
/* This is done to flush the socket */
(void) Ssock_recvall(ssock, buf, contentLength, 0);
free(buf);
}

HTTPServer_sendSimpleResponse(ssock, returnCode, contentType,
body ? strlen(body) : 0, body ? body : NULL);
}

return (status);
}

Thanks & Regards

Kalyan.