Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
I need to certificate HALCoGen, So I request and receive SafeTi-HALCoGen-CSP (Chip : TMS570LC4357)
When I test the sample project, there is an error occurred. But I don't know what is problem.
1. The Enviroment setting
- The complier changed : arm_5.1.6 -> ti-cgt-arm_18.1.4.LTS (Build Option :
Compiler Options: -mv7R4 --code_state=32 --float_support=VFPv3D16 --abi=eabi -g --diag_warning=261 --diag_warning=118 --diag_warning=225 --diag_error=189 --diag_error=994 --diag_error=551 --display_error_number --enum_type=packed Linker Options: --reread_libs --warn_sections --rom_model --be32 Run time Library: rtsv7R4_T_be_v3D16_eabi.lib CG Tool Root Path: C:\ti\ccsv8\tools\compiler\ti-cgt-arm_18.1.4.LTS
- LDRAUnit license ( LDRA license has already been purchased)
- OS ( Window 10 64bit)
2. The build error as followes.
- Error in "HALCoGenTAU"
- The Log file(ADC1_Unit test) :
Windows version [2:6:2] unknown! at D:/Perl/site/lib/Win32.pm line 218. LDRA Install Dir:C:\Program Files (x86)\LDRA\LDRAunit-TI-Qual_C_CPP_9.4.3\ Generating Make file for C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\TMS570LC43x\Sample_Projects\CSP_TMS570LC4357ZWT_Def\Test\ADC1\UnitTest\ADC1_UT.xlsx ... MakeFile Generation Passed Generating TCF file for C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\TMS570LC43x\Sample_Projects\CSP_TMS570LC4357ZWT_Def\Test\ADC1\UnitTest\ADC1_UT.xlsx....Name "main::Procedure" used only once: possible typo at C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\HALCoGenTAU\Scripts\Generate_TCF.pl line 744. Windows version [2:6:2] unknown! at D:/Perl/site/lib/Win32.pm line 218. Use of uninitialized value in pattern match (m//) at C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\HALCoGenTAU\Scripts\Generate_TCF.pl line 290. Use of uninitialized value in concatenation (.) or string at C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\HALCoGenTAU\Scripts\Generate_TCF.pl line 1311. Windows version [2:6:2] unknown! at D:/Perl/site/lib/Win32.pm line 218. LDRA Install Dir:C:\Program Files (x86)\LDRA\LDRAunit-TI-Qual_C_CPP_9.4.3\ Generating TCF :Passed Executing Testcase for C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\TMS570LC43x\Sample_Projects\CSP_TMS570LC4357ZWT_Def\Test\ADC1\UnitTest\ADC1_UT.tcf Windows version [2:6:2] unknown! at D:/Perl/site/lib/Win32.pm line 218. LDRA Install Dir:C:\Program Files (x86)\LDRA\LDRAunit-TI-Qual_C_CPP_9.4.3\ Windows version [2:6:2] unknown! at D:/Perl/site/lib/Win32.pm line 218. Use of uninitialized value in pattern match (m//) at C:\ti\Hercules\SafeTI-HALCoGen-CSP\TMS570LC43x_v04.07.01\HALCoGen\HALCoGenTAU\Scripts\Unit_Test_LDRA.pl line 129. Can't spawn "cmd.exe": No such file or directory at HCG_Unit_Test.pl line 375.