Other Parts Discussed in Thread: MSP-GANG
Questions about MSP-GANG programmer for programming MSP432P401R.
- From the user guide, it looks like Interactive mode is the only way to load binary files onto the programmer. Is this true?
- When we just have Go and Verify options enabled in the image file that is shared (the binary file is not shared), is it possible to copy the image onto the programmer?
- The user guide states that the only files supported on the SD Card are binary files (which are unencrypted). Is this true?
- Is the only security feature on the image file password protection or hardware fingerprint protection. Does the software encrypt the binary image as well so that even if the image is not password protected with only Go and Verify options enabled, then sharing the image file would ensure that the binary image cannot be reverse engineered from the image file.
Customer's goal is to keep their binary files secure, while allowing CMs to be able to update the image files on the programmer (if needed) easily.