Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Vit+ for Vcc=3.3V

Part Number: MSP432P401R

Hi,

I have a question from my customer.
What is Vit+ Max. value for Vcc=3.3V?
Our data sheet only provides values for Vcc=2.2V(1.65V) and Vcc=3V(2.25V).
Both are 75% of Vcc.


Vit+ for 3.3V is simply 75% of 3.3V, i.e. 2.475V?

Thanks and regards,
Koichiro Tashiro