This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Is it possible to use Pin J2 and R3 simultaneously as GIOB[6] ?

Part Number: TMS570LC4357

Hello Hercules Support-Team,

We are using the Pin J2 as nERROR, but we want to prevent the nERROR signal on J2 to go LOW on tests that trigger an ESM Error. So for the duration of the test we want to configure J2 as GIOB[6], which is already configured for Pin R3. During the test the state of R3 can be High. So we plan to configure GIOB[6] to be in state HIGH and then switch to J2 so that J2 and R3 output HIGH.

(Q1) Is it possible to configure GIOB[6] to be used simultaneously on PIN R3 and J2?

Thank you and best regards,
Max

  • Hello Max,

    Yes, both J2 and R3 can be configured as the output of GIOB[6] at the same time. If GIOB[6] is configured as input, only one of J2 or R3 can be used.

  • Hello QJ,

    Thank you for the quick answer. I have one follow up question.

    (Q2) What happens when R3 ist GIOB[6] Input and then J2 is switched to GIOB[6] also?

    Thank you and best regards,
    Max

  • Hello Max,

    The PINMMR87[8] and PINMMR[9] are used to select which pin is used as input to GIOB[6]. 

    If PINMMR87[8] is set and PINMMR87[9] is cleared, the terminal J2 is selected. If PINMMR87[8] is cleared and PINMMR87[9] is set, the terminal R3 is selected. 

    If both PINMMR87[8] and PINMMR87[9] are set or cleared, the Default Function (J2) will be selected as GIOB[6] input.