Part Number: MSP432E401Y
I would like to use two MSP432E UARTs at the same time, one reading while the other is writing, etc... and I'm not sure the best place to start. Should I:
I) convert all UART call to call-back, non blocking calls?
ii) convert my TI-RTOS tasks (one that R/W on UART0 and the other task handles R/W on UART7) to threads?
iii) I have the option to change one of the outputs to use the CAN port. Would it be easier to code one UART R/W and CAN R/W in parallel? If UART R/W with call-backs is the right answer, can you point me to an example that isn't just an echo?
Thank-you!