Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: GPIO state during reset

Part Number: MSP432P401R

Champs,

Customer would like to use the device to control power of the rest of the system and needs to make sure that during reset there is no possibility of a glitch on GPIO that would make it go high and mess with the system reset sequence. The datasheet says that GPIOs are in high impedance after POR but it doesn't specify their states during reset. To my understanding when device is held in reset the IO state should not change since the reset request is pending in the reset controller waiting for release but I don't see it definitely stated in the DS hence can not be 100% sure. 

Any insights will be greatly appreciated!

Michael