Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Using TExaS Display to probe an external circuit

Part Number: MSP432P401R

Greetings,

I have an external circuit on a breadboard (powered by an external SMPS) and I would like to probe it using the MSP432 P401R + TExaS Display software (the signals are <1kHz).

My questions are: Is it possible to do this? Do I need to connect the external SMPS ground to the MSP ground?

I tried probing an oscillator pin using a voltage divider (without joining grounds), it should have been a 2.5V square wave (since the pin is 5V and the resistors are equal in value) - but I got a 3.3V square wave instead. So I think there's a ground unbalance here, even though both the PC and the SMPS are at the same outlet.

Thanks in advance.