This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P4111: Reboot vs Hard reset: what does the boot code do that makes the difference?

Part Number: MSP432P4111
Other Parts Discussed in Thread: SYSBIOS, SYSCONFIG

Chris Sterzik mentioned : "The key difference between class 0/1 and class 2/3 is the boot code and the associated boot-override mailbox.  With class 0/1 the boot code is executed, where class ‘1’ is a ‘controlled’ re-execution of the boot code.   In this sense, with a hard reset the 'device' is not rebooted."

What does that boot code do? Is it in boot.asm file?