This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: connect with marvell switch

Part Number: TM4C1294NCPDT

Dear team,

My customer is using TM4C1294NCPD and 88E6190X (a chip from marvell).

At present, the customer hopes to realize the Ethernet function. Capacitive isolation is used on the circuit.

TM4C1294 needs to be pulled up to 3V3 through 49.9ohm, but marvell does not need to be pulled up.

After checking the information, I found that this is the connection of current type and voltage type phy. So if the pull-up resistor is not connected to the marvell side, How to modify TM4C1294?

Please help.