Part Number: EK-TM4C1294XL
Hi,
I am trying to learn about the bootloader using this link:
Here are the steps I tried:
1. Built boot_serial and used the flash button from CCS to download the bin file to EK-1294NCPDTXL
2. Built boot_demo 1 and used the flash button from CCS to download the bin file to the EK.
3. LED1 D1 starts blinking. I push the reset button SW1 on the EK and D1 stops blinking.
4. I use LM Flash programmer in manual configuration mode with serial UART interface,
autobaud support disabled. I try to flash boot_demo2.bin with program
address offset 0x4000. All erase buttons in the LM flash programmer are disabled in
this configuration.
The Flash programmer is failing to establish communication with the EK.
Why is this? Please explain so I can begin using the bootloader.
Thanks,
Priya