This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-RM57L: The GIO High-level interrupt does not work.

Part Number: LAUNCHXL2-RM57L

Hello

I run the same application on two development board: LAUNCHXL2-RM57L and TMDXRM57LHDK

The application manages 3 interrupts: one with GIOA[1] and two with GIOB[1] and GIOB[2].

GIOA[1] and GIOB[1] are configured with High-level interrupt.

GIOB[2] is configured with Low-level interrupt.

When the application is running on the TMDXRM57LHDK development board all is working well.

But when the application is running on the LAUNCHXL2-RM57L the 3 interrupts occur with the Low-level vector interrupt.

What can I do ? Where is the mistake ?

Thanks for your help

Jerome