This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to qualificate test about SafeTi Diagnostic Lirary using by TMS570LC4357.
So, I request SafeTi Diagnostic Lirary using by TMS570LC4357 in "Ti home page". I received "SafeTI Diagnostic Library-tau-TMS570LC43x-2.4.0_LDRA_Less-installer.exe"
Install this package, I can show the report of SafeTi Diagnostic Lirary using by TMS570LC4357 tested by Ti. But I need to test by myself.
when I try to test by myself, there are some problems,
First, my test environment.
1. Hardware : Our configured board (The board is made as ti guide. We already use the SafeTi Diagnosis Library well)
2. Software
1) Use the project in "SafeTI Diagnostic Library-tau-TMS570LC43x-2.4.0_LDRA_Less-installer.exe"
2) LDRAUnit set as the user guide.
3) Complier use "ccs8" -> so, the complier use "ti-cgt-arm_18.1.4.LTS"
The changed Test environment
1. Sci port : We use Sci port 4 in TMS570LC4357
1) I set bit 17 of sciREG4->GCR1 by following the guide ("HL_sci.c" in the root "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\demo_app\HALCoGen\TMS570LC4357_NoOS\source")
2) sciREG1 -> sciREG4 in "ldra_port.c" in the root "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\Test\TMS570LC43x\SafetyLibrary\Tests\source"
2. Change the Cmd file
-> Build is failed, when I use "SL_TMS570LC4357_NoOS_sys_link.cmd" in "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\Test\TMS570LC43x\SafetyLibrary\Tests\source"
So, I use "SL_TMS570LC4357_NoOS_sys_link.cmd" in "C:\ti\Hercules\SafeTI Diagnostic Library\2.4.0_LDRA_Less\build\TMS570LC4357_NoOS"
Then, the test is stopped following state,
The Debugger is stopped when system reset state.
Please let me know, why the system is stopped in this state.
Regards,
Minwoo
Hellog QJ Wang,
The problem is solved by make HalCoGen followed given CSP.
I think the test cases are optimized for CSP.
Thanks for your help
Regards,
Minwoo