Part Number: TIDM-BLPFC
Other Parts Discussed in Thread: CONTROLSUITE, TIDM-1007, C2000WARE
Hello,
I am Khalid Javed, a PhD Researcher from GHENT UNIVERSITY BELGIUM.
I have a TI Made Device i.e. TIDM BLPFC which is having a C2000 MCU. I already setup a connection between my laptop and the C2000 MCU with the help of the CCS and I did flashed the memory of the MCU. Now as TIDM- BLPFC is provided with a guide to understand the programing for the whole device under the link which is given below. So to understanding the process and to start with the BUILD 1, I have to import CCS Project into the CCS. So for that I am following the route i,e, when starting the CCS for the first timing and specifying the workspace I use the same directory i.e. C>ti>controlSUITE>development_kits>BLPFC_v1.0>BLPFC.
Then I go to the projects>import CCS project and then again from option of select search directory I use the same root directory i.e.
C>ti>controlSUITE>development_kits>BLPFC_v1.0>BLPFC.
It do loads the BridgelessPFC in discovered projects and I do select it,
But when I select finish then they appears the following error message.
Can you please guide me that where I am making mistakes?
Best Regards