Part Number: MSP432P401R
Hello,
I have a few queries on the BSL.
1. In the SW invocation method, the running firmware invokes the BSL. While BSL is updating the flash with the new firmware image, what would be the state of the IO pins that were configured by the running firmware, prior to invocation of the BSL. Would the IO pins continue to maintain their states?
2. After the firmware update is completed via SW invocation of BSL, is a reset of MSP432 required? Is it possible to update the firmware without disturbing the earlier configured states of the IO pins?
3. Can the BSL operate in I2C Master mode? I would appreciate if any pointers are provided on how this can be done.
Thanks in advance
Srikanth