Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Is ESM 2.24 generated when DWWD generates a nRST

Part Number: TMS570LC4357

Hello Support-Team,

We want to run the internal watchdog to be configured as DWWD. As reaction we want the DWWD to cause a nRST.

According to the Datasheet the a ESM 2.24 "RTI_WWD_NMI" is beeing generated, if the Watchdog is configured to generate an interrupt.

Q1) Is there an error signaled to the ESM and the nERROR pin set to LOW, when the DWWD causes a nRST?

Thank you and best regards,
Max