Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
I am trying the example prg of simple tx and rx program of CAN protocol which is available in Tivaware, I am using 120ohm resistor in this experiment, I have made the connection properly and bit rate for both tx and rx is 10000. Below attached is the output which i am getting, kindly let me know the necessary changes need to done