Part Number: MSP432P401R
Hello,
I am having issues connecting my launchpad to my linux PC. I have both CCS 9.3.0 and CCS 10.2.0 installed; neither can communicate with the launchpad and the same error is returned:
[Start] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ /home/w/.ti/ccs930/0/0/BrdDat/testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100- or 510-class product. This utility will load the adapter 'libjioxds110.so'. The library build date was 'Jan 31 2021'. The library build time was '22:02:59'. The library package version is '9.3.0.00042'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-260' (0xfffffefc). The title is 'SC_ERR_XDS110_OPEN'. The explanation is: An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. [End]
I've tried grounding tdo and unplugging and reconnecting the launchpad, but it's still not recognized.
When I run the lsusb command to list USB devices, I get the following output (showing only relevant info):
$ lsusb
Bus 001 Device 017: ID 0451:bef3 Texas Instruments, Inc. CC1352R1 Launchpad