Part Number: EK-TM4C123GXL
Can I get the programmer hex-file on the EK-TM4C123GXL board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EK-TM4C123GXL
Can I get the programmer hex-file on the EK-TM4C123GXL board?
Hello Sergei,
If you mean the out of box example, that is the qs-rgb example in TivaWare which can be found at [Install Path]\TivaWare_C_Series-2.2.0.295\examples\boards\ek-tm4c123gxl\qs-rgb. If you meant something else, please provide more details here because it is unclear what else you might be looking for.
Hello, Ralph!
There is a programmer on the board ek-tm4c123gxl. The programmer broke down. I installed a new chip. I want to restore his program.
Hello Sergei,
Ahh okay now I understand. Thank you.
We don't give out the hex file but you can re-program the board with LM Flash Programmer.
Once you plug in your LaunchPad, select it from the Configuration options and then go to 'Other Utilities'. At the bottom of that tab, you will find an 'ICDI Firmware Update' section. Use the Update feature there, and the LM Flash will load a new ICDI image onto the device.