Part Number: UNIFLASH
Other Parts Discussed in Thread: MSP-EXP430G2ET, , MSP430G2553
Hello, I have been trying to get the uniflash program to flash a .hex file (built in CCS V10) onto a MSP430G2553 microcontroller. I have had success with flashing the program on the MSP430G2553 chip using the MSP-EXP430G2ET launchpad. However, when I try using a FTDI FT232RL USB-Serial converter (set to 3.3V logic level for serial communications) to flash the MSP430G2553 chip I get a readout in the console section stating that "the response byte for sync command from bootloader is not recieved" and an error message; both are shown in the below image. Any advice on what is causing this error would be greatly appreciated.
Sincerely yours,
Jeremy
Hook up of FT232RL breakout board to MSP430G2553 chip:
FT232RL MSP430G2553
RX ---------> TX
TX --------> RX
DTR --------> RST
RTS --------> TEST
3.3Vdc -------> 3.3Vdc
GND -------> GND