Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-RM57L: SDI with RM57

Part Number: LAUNCHXL2-RM57L

Good morning

I have a great doubt, reviewing the user manual of the RM57L, found that it has a type of communication "2-Data Line Mode".

which I would like to take advantage of to communicate with a 23LC1024 RAM memory brand Microchip.

Previously, I already communicated normally, only now to gain speed I would like to use the SDI memory mode.

have problems with understanding the connection of the external pins.

Best Regards

Martin Valencia

  • Hi Martin,

    As the TRM says that in 2-data line mode (master mode) the shift register bits 15 and 7 will be connected to the pins SIMO[1] and SIMO[0], and the shift register bits 8 and 0 will be connected to the pins SOMI[1] and SOMI[0]. If you use SPI parallel mode, you have to swizzle the data to meet the communication protocol of SDI mode of 23LC1024.

    SDI mode protocol: