Part Number: TM4C1290NCPDT
Hello,
We are using TM4C1290NCPDTT3 in one of our design and the boot image stored in its internal flash memory. Normally it is booting and the application image is running good with no issues. Once in a while it failed to boot and when we simulated power cycle test, observed it failed to boot 10 out 10000 power cycle. When it failed to boot, asserting system reset on the pin-70 (RST) is not doing anything and remains hang. Tried to connect with JTAG via code composure studio and it failed to connect. It requires power cycle to get it back to working. Normally JTAG connections are working good and asserting reset pin, resets the application image running in microcontroller. Not sure what am I missing in the design, appreciate your help to resolve this issue. Not sure is this a known behavior with this controller..?
We are using 13MHz external clock and the reset will be released after 1second from power-ON. The +3.3V voltage looks good with power-up ramp 10uS and 13MHz clock is looking good when the reset is released after 1second from power-ON. This failure is occurring randomly and its happening in all the boards we built (~20-Boards) at both +75'C and -40'C temperature.
Thanks,
Boopathy