This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: ultrasonic hc sr-04 with tms570ls1224

Expert 1660 points

Part Number: TMS570LS1224

Hello everyone is there any examples on implementing ultrasonic hc sr-04 with tms570ls1224

  • Hello,

    You can use either N2HET or ePWM or GIO to generate a 10us trigger pulse for HC-SR04, and use GIO or eCAP or N2HET to capture the rising and falling edge of the echo output from the HC-SR04. RTI can be used as the timer which counts the time between the rising edge and falling edge of the echo input signal.

    I don't have examples, but it is not hard to implement.

  • hello QJ,

    i connected N2HET1[10]  to the sensor trig

    and N2HET1[30] to the sensor echo.

    in halcougen i just enabled het1 and  GIO .

    i also enabled het1 in PINMUX

    and then went to het 1 (pwm 0-7)  in PWM 1 , I changed the period to 10us and selected pin 10 as output pin, and enabled PWM SIGNAL AFTER HETINIT.   in here do i need to change the duty cycle????

    then in cap0 i changed the low polarity to high polarity and set pin 30 .

    then i went to (pin 8-15) and enabled output direction for bit 10 . In (pin 24-31) i select bit 30 as pullup

    about the code

    
    

    #include "het.h"
    #include "sys_common.h"
    #include "gio.h"
    
    hetSIGNAL_t  duration;
    
    
    float distance;
    
    void main(void)
    
    {
    
        while(1){
        
        hetInit();
        gioInit(); 
    
        gioSetDirection(hetPORT1, 0xBFFFFFFF); // 30 Input, 10 Output 
        
    
       
    gioSetBit(hetPORT1, 10, 1); 
    
    
        pwmSetDuty(hetRAM1, pwm0, 10U);
        pwmStart(hetRAM1, pwm0);
    
     capGetSignal(hetRAM1,cap0, &duration);
    distance =( duration.period * 0.034) / 2;
    
    }
    
    }

     

  • Please see my reply:

    e2e.ti.com/.../3626368