Part Number: MSP432E401Y
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I'm using a MSP432E401Y with an external ULPI.
In the sysconfig file, I've got a conflict on 3 pins, but I won't use them, as the ULPI will be used to control VBUS and I don't have an ID pin.
The ID and VBUS conflicts cannot be solved, as the only pins I can choose are the ones I need for a CAN bus.
Should I ignore this conflict ? Why are these pins mandatory even when High-Speed is selected ? (It seems like I can't just disable them)
I also won't use the D- and D+ pins, what should I do with them ?
Here's a screenshot of my syscfg file.
Thank you very much.
Have a nice day.
Victor Tolosana