Part Number: EK-TM4C129EXL
Hi
As the title states I am seeing different results if I run the TivaWare_C_Series-2.2.0.295 enet_tcpecho_server example for the EK-TM4C129EXL in Code Composer Studio then when I run it in IAR Systems EWARM.
As the code comments state (since SW-EK-TM4C129EXL-UG-2.2.0.295 is particularly vague on usage) I have created a TCP connection on telenet port 23 to the IP address provided using PuTTY, if i run this example in IAR EWARM I pretty quickly observe a FaultISR(), in CCS no such fault occurs and connection stays up and operates as expected.
This has not been the only strange/buggy behaviour that I have observed when running the examples in IAR EWARM, including but not limited to, verify error at address warnings when downloading and debugging and hitting the hardfault ISR straight out of the blocks. Please advise.