Part Number: TMDSEMU110-U
I want to mount the TMDSEMU110-U
I need the perimeter dimensions, and mounting hole (if any) dimensions.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSEMU110-U
I want to mount the TMDSEMU110-U
I need the perimeter dimensions, and mounting hole (if any) dimensions.
Hi Bryan,
The TMDSEMU110-U comes in a plastic enclosure. I've attached the dimensions I've found (all dimensions are in inches). There are no mounting holes that I can see. Is this what you were looking for?
EDIT: To avoid confusion for future readers, clarified in later post these were NOT the enclosure drawings & removed drawings.
Gus, I noticed that the 2.145 dimension conflicts with the 2.315 dimension. Which is correct?
Bryan
Sorry, I misinterpreted the drawings. These are markings/overlay for the enclosure, not the actual enclosure dimensions. I'm not able to find a drawing for the actual enclosure. The build materials list mention a 3.6 X 2.6 X 1.1 enclosure. I'll see if can find more information.
Bryan,
The link below contains the dimensions of the enclosure.
Note: The actual part used is made of different plastic.