Part Number: TMS570LS1114
Dears
please help me to check the code as below, my issue is that IF3 data cannot be synchronized with IF2 !
#include "all_header.h"
#include "system.h"
#include "emif.h"
#include "errata_SSWF021_45.h"
#include "etpwm.h"
#include "sys_dma.h"
#include "reg_etpwm.h"
#include <stdio.h>
#include <string.h>
static uint32_t Received_ID ; /*SD_20210119*/
static uint32 DMA_Comp_Flag;
g_dmaCTRL g_dmaCTRLPKT; /*dma control packet configuration stack*/
#define D_COUNT 8
#define D_SIZE 8
int data;
uint32 cnt = 0;
uint32 error = 0;
uint32 tx_done = 0;
uint32 CpuCount = 0;
uint32 timer0 = 0;
uint8_t tx_data1[D_COUNT] = {1, 2, 3, 4, 4, 3, 2, 1}; /*transmit buffer in sys ram*/
uint8_t tx_data2[D_COUNT] = {1, 3, 5, 7, 9, 11, 13, 15};
uint8_t tx_data3[D_COUNT] = {2, 4, 6, 8, 10, 12, 14, 16};
uint8_t rx_data[D_COUNT] = {0};
uint8_t rx_data1[D_COUNT] = {0}; /*receive buffer in sys ram*/
uint8_t rx_data2[D_COUNT] = {0};
uint8_t rx_data3[D_COUNT] = {0};
void delay(uint32 time);
void dmaConfigCtrlRxPacket(uint32 sadd,uint32 dadd,uint32 dsize);
uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize);
void dmaGroupANotification(dmaInterrupt_t inttype, uint32 channel)
{
DMA_Comp_Flag = 0x5555AAAA;
}
void delay(uint32 time)
{
int i;
for(i = 0; i < time; i++)
;
}
void main(void)
{
_enable_interrupt_(); /*Enable IRQ interrupt in ARM CPSR register*/
DMA_Comp_Flag = 0xAAAA5555; /* Reset the Flag */
rtiInit();
rtiEnableNotification(rtiNOTIFICATION_COMPARE0);
// rtiDisableNotification(rtiNOTIFICATION_COMPARE0);
_enable_IRQ();
rtiStartCounter(rtiCOUNTER_BLOCK0);
u8gv_tmr_addr = get_tmr_addr();
canInit(); /* initialize can*/
vimInit();
canREG1->CTL |= (uint32)(1<<18); /*enable DMA DE1 for IF1*/
canREG1->CTL |= (uint32)(1<<19); /*enable DMA DE2 for IF2*/
canREG1->CTL |= (uint32)(1<<20); /*Enable DE3 bit in CTL register to trigger DMA when IF3 receives data*/
canREG1->IF3OBS = 0x0000001AU; /* Read ARB, DATA A & B - 8 bytes */
canREG1->IF3UEy[0] = 0x0000002AU; /*Message box of RX 2,4,6 configured for auto update*/
/* - DMA Configuration */
dmaEnable(); /* Enable DMA */
// dmaEnableInterrupt(DMA_CH16, FTC); /*Enable Interrupt after reception of data*/
dmaEnableInterrupt(DMA_CH0, FTC);
// dmaReqAssign(DMA_CH2,17); /*DMA Configuration and Enable DMA:DCAN1 IF1对应DMAREQ[17]*/
// dmaReqAssign(DMA_CH1,6); /*DCAN1 IF2对应DMAREQ[6]*/
dmaReqAssign(DMA_CH0,16); /*DCAN1 IF3对应请求线DMAREQ[16]*/
// canEnableloopback(canREG1, Internal_Lbk);
/* - Populate dma control packets structure */
/* Source Address = IF3 Data register
* Destination = Receive Buffer in Sys RAM
* Length = 1 ( 64bits = 8 * 8 Bytes)
*/
// dmaConfigCtrlRxPacket((uint32)(&tx_data2), (uint32)(&(canREG1->IF1DATx[0])), 1);
dmaConfigCtrlRxPacket((uint32)(&(canREG1->IF3DATx[0])),(uint32)(&rx_data2),1);
// dmaConfigCtrlRxPacket((uint32)(&rx_data2),(uint32)(&(canREG1->IF2DATx[0])),1);
dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT); /*setting dma control packets for transmit*/
// dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT);
// dmaSetCtrlPacket(DMA_CH2, g_dmaCTRLPKT);
dmaSetChEnable(DMA_CH0, DMA_SW); /*CH0使能,IF1填充数据*/
// dmaSetChEnable(DMA_CH1, DMA_SW);
#if 1
while(1)
{
// printf("CAN TX\n");
delay(100000);
DMA_Comp_Flag = 0xAAAA5555; /* Reset the Flag */
canTransmit(canREG1, canMESSAGE_BOX3, (const uint8 *)&tx_data2[0]); /* transmit on can1 */
// canIsTxMessagePending(canREG1, canMESSAGE_BOX3);
CpuCount = canIsTxMessagePending(canREG1, canMESSAGE_BOX3);
// can1LowLevelInterrupt();
// can1HighLevelInterrupt();
while(!canIsRxMessageArrived(canREG1, canMESSAGE_BOX4))
;
dmaFTCAInterrupt();
while(DMA_Comp_Flag != 0x5555AAAA); /* Wait for the DMA interrupt ISR to set the Flag */
canGetData(canREG1, canMESSAGE_BOX4, (uint8 *)&rx_data[0]); /* receive on can1 */
Received_ID = (canREG1->IF3ARB & 0x1FFC0000)>>18;
}
#endif
return 0;
}
void canMessageNotification(canBASE_t *node, uint32_t messageBox)
{
while(!canIsRxMessageArrived(canREG1, canMESSAGE_BOX4))
;
canGetData(canREG1, canMESSAGE_BOX4, (uint8 *)&rx_data[0]);
Received_ID = (canREG1->IF3ARB & 0x1FFC0000)>>18;
/*
switch(rx_data[0])
{
case 13:
data = (rx_data[1] - 0x30) * 1000 + (rx_data[2] - 0x30) * 100 + (rx_data[3] -0x30) * 10 + rx_data[4] - 0x30;
data *= 1.25;
break;
default:
break;
}
etpwmREG1->CMPA = data;
memset(rx_data, 0, sizeof(rx_data));
data = 0;
*/
}
#pragma WEAK(rtiNotification)
void rtiNotification(uint32 notification)
{
/* Reset the Flag */
timer0 ++;
}
void dmaConfigCtrlRxPacket(uint32 sadd,uint32 dadd,uint32 dsize)
{
g_dmaCTRLPKT.SADD = sadd; /* source address */
g_dmaCTRLPKT.DADD = dadd; /* destination address */
g_dmaCTRLPKT.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT.FRCNT = 1; /* frame count */
g_dmaCTRLPKT.ELCNT = dsize; /* element count */
g_dmaCTRLPKT.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.ELSOFFSET = 0; /* element source offset */
g_dmaCTRLPKT.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.FRSOFFSET = 0; /* frame source offset */
g_dmaCTRLPKT.PORTASGN = 4; /* port b */
g_dmaCTRLPKT.RDSIZE = ACCESS_64_BIT; /* read size */
g_dmaCTRLPKT.WRSIZE = ACCESS_64_BIT; /* write size */
g_dmaCTRLPKT.TTYPE = FRAME_TRANSFER ; /* transfer type 一个请求触发一帧传输 */
g_dmaCTRLPKT.ADDMODERD = ADDR_FIXED; /* address mode read */
g_dmaCTRLPKT.ADDMODEWR = ADDR_FIXED; /* address mode write */
g_dmaCTRLPKT.AUTOINIT = AUTOINIT_ON; /* autoinit */
}
/* USER CODE END */