Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: DP83630
Hi All,
Currently, we are trying for the TI example program using Launchpad XL2 RM57 <=> Launchpad XL2 RM57.
This board consists of DP83630 Ethernet PHY Transceiver IC. We are able to establish the physical & Link Layer.
Below are the configurations,
# MII Mode with 100 Mbps with Internal reference Clock
# ACT & LINK LEDS are ON
# VCLK4=40MHz(or)75 MHz=> We are getting the same behaviour for the both the clock
# Channel 0
# BROADCAST addressing
# MAC ADDRESS(Point to Point.There is no IP address configured as of now. Sending the packets in Broadcast MAC address)
# Phy address=0x01 for the both the launchpad XL2-RM57
https://e2e.ti.com/support/interface/f/138/t/835939
As per Aniruddha feedback given in the above link,
RX_ER high indicated that there was some invalid symbols received during the data transfer.
False Carrier and RX_ER can indicate towards a reference clock issue.
Hence, we have taken the measurements in CRO. Does this captured signal behaviours are OK? Herewith I have attached my Transmit Code/Receive for the reference.
Regards,
S.Saravanakumar