Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN
Hello,
I want to generate a PWM signal with the ePWM module.
I use the halcogen function 'etpwmsetcmpA(..)' to control the pwm output. This works fine so far.
But when I want to set the PWM to zero, one full PWM period with a duty cycle of 100% occurs. (See attachment)
What is the reason of this behavior? How can I create a direct zero on the output?
Thanks
Daniel Diener