Part Number: MSP432P401R
Hi Team,
Please provide the maximum full active current consumed by the microcontroller MSP432P401RIPZR with 3.3V power supply.
Thanks,
Denny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Denny,
Sorry for the delayed response. PLease see sections 5.10, 5.11, and 5.12 of the datasheet for the active mode current consumption specifications.
Thank you Eddie. So with VCC=3.0V, MCLK = 48 MHz, the max current consumption is just 8400uA or 8.4mA. With mentioned conditions like: all the other input pins tied to 0 V or VCC and peripherals are inactive,.. etc.
So the total current consumption is very less, i.e less than 10mA.
Thanks,
Denny