Part Number: ARM-CGT
Hello,
Didn't know marking the issue as resolved close the thread so its continuation of the post e2e.ti.com/.../3632413
which George resolved but I have some followup question, If you think it opening too many threads you can collapse it into one or place this appropriately,
Thanks George,
I have another set of followup question, May you please be kind in answering those
- Do I need to add any header files to use this intrinsic sets and also if I want to use e ARM C Language Extensions (ACLE) specification, only including the arm_acle.h along with correct core selection like -mv7m3 (for m3 ) and -mv7r4 (for R4 ) will work?
- I am facing one strange issue in compilation,
- When I select the R4 core with Big endianess(along with the correct lib rtsv7R4_T_be_eabi.lib) the compilation is successful
'Building target: aaa_M4.out'
'Invoking: ARM Linker'
"E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=32 -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=packed --abi=eabi -z -m"aaa_M4.map" --heap_size=0x800 --stack_size=0x800 -i"E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib" -i"E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="aaa_M4_linkInfo.xml" --rom_model --be32 -o "aaa_M4.out" "./IntMathLib/IntMathLib.obj" "./aaa/aaa_NoiseEstimation.obj" "./aaa/aaa.obj" "./mss_data.obj" "./main.obj" "./Unit_Test_aaa.obj" "./FileRead.obj" -l"rtsv7R4_T_be_eabi.lib"
<Linking>
warning #10247-D: creating output section ".text" without a SECTIONS specification
warning #10247-D: creating output section ".const" without a SECTIONS specification
warning #10247-D: creating output section ".data" without a SECTIONS specification
warning #10247-D: creating output section ".bss" without a SECTIONS specification
warning #10247-D: creating output section ".cinit" without a SECTIONS specification
warning #10247-D: creating output section ".sysmem" without a SECTIONS specification
'Finished building target: aaa_M4.out'
b. When I change the endianess to my targeted one little endianess with the lib rtsv7R4_T_le_v3D16_eabi.lib my compilation fails
"E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=32 -me -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=packed --abi=eabi -z -m"aaa_M4.map" --heap_size=0x800 --stack_size=0x800 -i"E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib" -i"E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="aaa_M4_linkInfo.xml" --rom_model -o "aaa_M4.out" "./IntMathLib/IntMathLib.obj" "./aaa/aaa_NoiseEstimation.obj" "./aaa/aaa.obj" "./mss_data.obj" "./main.obj" "./Unit_Test_aaa.obj" "./FileRead.obj" -l"rtsv7R4_T_le_v3D16_eabi.lib"
<Linking>
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<boot.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<ll_lsl_t2.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<memcpy_t2.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<memset_t2.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<u_div32.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<_printfi.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<_scanfi.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<s_frexp.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<s_scalbn.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<strtod.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<ull_div32.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<ll_mul_t2.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
error #16004-D: file "E:/workspace_v5_5/ti-cgt-arm_16.9.6.LTS/lib/rtsv7R4_T_le_v3D16_eabi.lib<s_copysign.obj>" has a Tag_ABI_VFP_args attribute value of "1" that is different than one previously seen ("0"); combining incompatible files
warning #10247-D: creating output section ".text" without a SECTIONS specification
warning #10247-D: creating output section ".const" without a SECTIONS specification
warning #10247-D: creating output section ".data" without a SECTIONS specification
warning #10247-D: creating output section ".bss" without a SECTIONS specification
warning #10247-D: creating output section ".cinit" without a SECTIONS specification
warning #10247-D: creating output section ".sysmem" without a SECTIONS specification
error #10010: errors encountered during linking; "aaa_M4.out" not built
>> Compilation failure
gmake: *** [aaa_M4.out] Error 1
gmake: Target `all' not remade because of errors.
For Point there is no change in code except the correct endianess and corresponding Lib change which is intended and for this I intend to use ti-cgt-arm_16.9.6.LTS compiler.
Thanks again for your continued support