Part Number: RM57L843
Other Parts Discussed in Thread: LM629, LAUNCHXL2-RM57L, MOTORWARE, HALCOGEN
Some 12 years ago I used venerable LM629 with C8051F043 and isolated CAN2, mosfet H bridge to position low mech. time constan,t ironless capstan brushed DC motor.
Having LAUNCHXL2-RM57L and DRV8432 now, my questions are;
1) Can I fully emulate pair of LM629's full position PID's with RM57L resources ?
2) If so, what would be estimated positioning loops frequency?
3) To old to waste remaining R&D resources in reinventing the wheel, is there full positioning PID sample code in TI Motorware or HALCOGEN for RM57L, LM629 style ?
4) since LM629 is still in TI listed product line, shall such RM57 setup outperform it ?
Positioning PID loops shall do, dual optical A/B encoder inputs and sign/magnitude outputs are worth rethinking then.
Cheers,
Petric