This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Enquiry for suitable Micro controller



Hello,
For my internal project, I need a micro controller with the following requirements
    1) Industrial grade
    2) PWM outputs - min 2 Nos
    3) Max PWM output clock - 500KHz (input clock to be selected accordingly)
    4) Supports 1Gbps Ethernet port - 1 No. (It could be either with internal MAC & PHY or with external PHY and connected thru a suitable interface to the MCU).
Kindly please update the response as soon as possible.
Thank you