Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU for multiple slave bluetooth

Genius 9880 points

Hi Team,

Good day.

Customer is looking for MCU that can help with they application. 

Customer need to create a multi slave Bluetooth connection and would like to know if is possible with our MCU.

All the slaves are smartphone or personal devices.

"

Details of the system:


Central audio mixer with several headset connected. I want to place a Bluetooth master device inside this central audio mixer.

The user connected with the headset will have the possibility to connect the personal device to the audio center mixer in order to listen the music or conduct phone call.

"

Regards,

Maynard

  • Which Bluetooth device are they planning to use? Is it TI Dual mode CC2564x device? With regard to MCU for audio mixing etc, they may need audio DSP capabilities.. Please check with the MSP team, if they have a solution for audio mixing functionalities etc..

    Thanks