Part Number: TMS570LS3137-EP
Hi
For some reason, I couldn't upload images in my previous thread. Hence, I created this related thread to add the screenshots.
As shown in below screenshots, there is a 'default' word delay of 118ns between two 16-bit words on the CS line when WDEL = 0 (bit-26 in TxRAM) whereas word delay of 342ns is introduced if WDELAY is set to 1 in SPIFMT0 register and WDEL = 1.
WDEL = 0

WDEL = 1

It is not clear what setting in DMA/SPI is causing this default delay of 118ns.
Could you please clarify.
Thanks,
Jai