Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
Hello everyone,
I am trying to control a linear actuator using a Tiva TM4C123G6HPM microcontroller and a motor driver.
I am generating a 250 HZ PWM signal at 100% duty signal and have connected that pin to the appropriate enable pin on the motor driver.
I have two output pins on the microcontroller that connect to two pins of the motor driver to control the direction of the motor. The problem I am having is that when the output pins of the microcontroller are low and not sending a voltage of 3.3V to control the direction, the direction pins on the motor driver are still getting activated. The manual of the motor driver says that the pins need a voltage of at least 3V to get activated, but I measured the voltage of the microcontroller pin at low and its about 6.3mv , which is enough to activate the pin on the motor driver.
Does anyone know how I can fix this?
Thanks!