Part Number: C2000-CGT
Hi TI expert
The forums are erroring out on me, so I gave up... here are a few typos that I found.
In SPRUHS1C pg 793
The title "QUADF32 RaH, RbH, RcH" is missing the second input RdH, which is for the x-value. There is even a description of the D-register in the operands section below.
In SPRU514V pg 170
The inputs for the intrinsic operator "float __atan2puf32( float x, float y );" are swapped in the documentation, it should be: "float __atan2puf32( float y, float x);" This was tested to be the case with 20.12.0.STS
Best regards,
Thomas