Part Number: UNIFLASH
Other Parts Discussed in Thread: CC3235SF
Hi,
I am working on CC3235SF LaunchXL Dev Kit. I am trying to use Uniflash CLI to flash my binary. I have performed the following steps.
1. Generate my application .bin file in Code Composer Studio.
2. Import the .bin file in Uniflash and generate the SLI file.
3. Select Standalone Command Line in Uniflash and clicked Generate Package to generate the .zip file.
4. Connected my CC3235SF Dev Kit to the PC.
5. Extracted the .zip file
6. Executed the dslite.bat file in order to flash the binary. I see the failure as seen below in the highlighted line.
Executing default command:
> dslite --mode serial -c user_files/configs/CC3235SF_BL.ccxml -l user_files/settings/generated.ufsettings -s VerifyAfterProgramLoad="No verification" -e -f "user_files/images/TI_App.sli,1"
DSLite version 10.1.0.2076
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: Cortex_M4_0
Executing Startup Scripts: Cortex_M4_0
Connecting...
Loading Images...
info: Cortex_M4_0: CC3235SF(Bootloader)
info: Cortex_M4_0: ...Start to invoke the bootloader...
info: Cortex_M4_0: Trigger XDS reset
Failed: Image loading failed: CreateProcess failed: The system cannot find the file specified.
I am not sure why this failure is seen since the image is present in the user_files\images directory.
It works if I flash directly from the Uniflash tool. Only CLI does not work.
Any help/suggestion on how to resolve this is deeply appreciated.
Thanks and Regards,
Subramanyan