Other Parts Discussed in Thread: TMDS570LS31HDK, HALCOGEN
Hello,
I am evaluating an option to use HALCoGen-CSP for TMS570LS31x21x version 04.07.01. I am using TMDS570LS31HDK and I would like to ask the following questions:
1. I was able to execute test cases using HALCoGen TAU tool and get Regression and Dynamic Coverage Analysis reports. However, I have not got the outputs from static analysis, Code Review and Quality reports, and the Traceability Matrix. I assume some additional steps are required to be performed to get these outputs. Is there any description or guidance for these steps please?
2. I successfully executed unit tests, but the functional tests were not executed as I would expect. For example, the execution of ADC1_FT got stuck in the beginning and I had to kill the process. The User Guide SPNU633, section 12.9 describes there is a definition of not applicable test cases for a particular configuration in the documentation. I am aware it is not possible to run functional tests for modules that are not enabled in HALCoGen project, but is there any other limitation causing this issue?
3. As I was looking at the test case Excel files, I found some inconsistencies e.g. Df_type attribute is not defined for ADC1_UT, tests cases ADC1_UT_03:1 - ADC1_UT_04:3. Is this an intention or a defect? I would expect that this attribute is mandatory for LDRAunit.
Thank you for your response,
Peter