Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: UNIFLASH, RM46L852
Hello,
We are using Code Composer Studio v9.1.0, XDS110 debuggers, and UniFlash v5.3.1 to develop, debug, and flash our boards that run with RM46L852 MCUs. Our development environment is Linux Ubuntu 18.04.3 LTS.
The emulation package that is installed on the XDS110 debuggers is 8.2.0.00004. But some of the debuggers cannot program our boards using UniFlash and they require the emulation package to be updated to 8.4.0.00006, while some of our debuggers do not have this issue. We use the standard steps to program a debugger:
1. ./xdsdfu -e
2. ./xdsdfu -m
3. Connect to Luminary Micro Device Firmware
4. ./xdsdfu -f firmware.bin -r
5. The update is always successful.
How can we resolve this issue?
Thanks,
Peman