Other Parts Discussed in Thread: CC2520, CC2500, CC2652RSIP, CC2650MODA, CC2652P, CC1352P
Hi Team,
Our customer is going to develop a radio controller for drone application. The generic specifications of the radio controller are as follows.
Frequency = 2.4 GHz, they could consider a lower band later such as 868 MHz (EU).
Maximum TxPower = up to 20 dBm for maximum range
Package = Module with antenna
According to the customer the RC communication protocol will be chosen afterwards depending on the IC. Some companies are using IC's such as the TI CC2500 and TI CC2520.
It seems that our RF modules are for bluetooth and WiFi applications only. Do we have an RF module which he can use for radio control?
Regards,
Danilo