This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123BH6ZRB: What does Rs and Radc mean for application?

Guru 65710 points
Part Number: TM4C123BH6ZRB

Hello

In the data sheet, it mentions that the Rs is Max at 500ohms and Radc is max at 2.5Kohms.

What does these two parameters mean? how do they impact customer's design to get a better ADC accuray?

Thanks

Yihe

  • Hello Yihe,

    These values go along with Figure 13-7. ADC Input Equivalency in the device datasheet.

    As for how to use this information to improve ADC accuracy, I would suggest they read through the follow application note about ADC source impedance: www.ti.com/.../spna061.pdf

  • Hi 

    Thanks for the application notes. it does not explain the function of the Radc. if customer has a external voltage divider, will the Radc impact the voltage divider?

    Regards

    Yihe

  • Radc is the converter's intrinsic input impedance. It is what the external driver sees.

    Yes, Radc affects the external voltage divider.

    If the customer needs a voltage divider in front of the converter to, for example, reduce the range of an input signal that would otherwise exceed the ADC input, then buffer the divider with an op-amp. The converter then sees the low source impedance it prefers.

  • Just to add to Andy's post, the Radc resistance is between the pin and the sample capacitor. It will affect the time for the sample capacitor to charge or discharge along with your external source resistance. Once the sample capacitor is at the same voltage as the external pin, it will not affect the voltage divider (input leakage is small). 

    In short, you can ignore Radc when you calculate the resistor divider to determine the voltage range, but you must consider Radc when you calculate your minimum sample time. Adding the external capacitor will really help with the sample time as explained in the application note. It does act as a low pass filter so that needs to be taken into account.