Part Number: TMS570LS0714
hi
I am using fee driver with TMS570LS07 and I realy need help to know how i can erse all the block or the adress i want in eeprom
I tried the code below but it does not work so please can any one help me
my code is here
#include "ti_fee.h"
#include "sys_common.h"
#include "system.h"
uint16 u16JobResult,Status;
Std_ReturnType oResult=E_OK;
unsigned char read_data[100]={0};
uint8 SpecialRamBlock[100]={30,31,32,33};
unsigned char pattern;
uint16 u16writecounter;
unsigned int FeeVirtualSectorNumber;
unsigned char VsState, u8EEPIndex;
unsigned char u8VirtualSector;
uint8 Test_Recovery;
uint8 Test_Cancel;
uint8 *adress_of_block;
void delay(void)
{
unsigned int dummycnt=0x0000FFU;
do
{
dummycnt--;
}
while(dummycnt>0);
}
void main(void)
{
/* USER CODE BEGIN (3) */
unsigned int BlockNumber;
unsigned int BlockOffset, Length;
unsigned char *Read_Ptr=read_data;
unsigned int loop;
/* Initialize RAM array.*/
//for(loop=0;loop<100;loop++)SpecialRamBlock[loop] = loop;
/* Initialize FEE. This will create Virtual sectors, initialize global variables etc.*/
TI_Fee_Init();
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
}
while(Status!= IDLE);
TI_Fee_EraseImmediateBlock((uint16_t)0xF02001D8);
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
}
while(Status!=IDLE);
/* Write the block into EEP Asynchronously. Block size is configured in ti_fee_cfg.c file. Default Block size is
8 bytes */
BlockNumber=0x1;
TI_Fee_WriteAsync(BlockNumber, &SpecialRamBlock[0]);
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
}
while(Status!=IDLE);
// //here block number is our start block to write then our buffer will fill the blocks which after him untill
// //our buffer write all its data
BlockNumber=0x1;
/* Write the block into EEP Synchronously. Write will not happen since data is same. */
// TI_Fee_WriteSync(BlockNumber, &SpecialRamBlock[0]);
BlockOffset = 2;
Length = 0xFFFF;
oResult=TI_Fee_Read(0x1,BlockOffset,Read_Ptr,Length);
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
}
while(Status!=IDLE);
/* Invalidate a written block */
// TI_Fee_InvalidateBlock(BlockNumber);
// do
// {
// TI_Fee_MainFunction();
// delay();
// Status=TI_Fee_GetStatus(0);
// }
// while(Status!=IDLE);
/* Format bank 7 */
//TI_Fee_Format(0xA5A5A5A5U);
while(1);
/* USER CODE END */
}

i tried to delete all of that data but i could not i just need to know how to erase full memory or data of an address