Part Number: MSP432E411Y
Dear team,
My customers want to use EPI to connect external Flash and SDRAM. They have many questions. Please help to check them.
Because customers need to use the third-party file system fatfs, they want to use its unicode encoding. They need to include a unicode array close to 2M into the program. Customers now have some questions.
Assume:MSP432 expands flash, for example, it expands 32M flash.
1. Whether the off-chip flash can save the initialized array data.
2. Can the program be executed directly from the off-chip flash.
3. Will the addressing speed of the off-chip flash be slow or the reading and writing speed will be slow?
4. I found that, for example, SDRAM and flash can be expanded to a large extent, so without considering the cost of the product, there will be any problems if the expansion is too large. In addition to the power consumption, I would like to know the impact.
5. If I need to sleep MSP432 under low power consumption, do I not use SDRAM but use SRAM, because I can power SDRAM or SRAM alone, but I cannot refresh SDRAM because MSP432 is already dormant, so I need to use SRAM, am I right?
6. Can the EPI interface expand Flash and SRAM at the same time?
Thank you!