Part Number: TM4C1294NCPDT
Hello,
A new topic, I developed an application with Ethernet in using the library lwiplib.(easy)
Now I would like to use TI RTOS because my system is more complex with 1 Ethernet, 5 UART...
I tested the example tcpEcho but it is more difficult because I need to select DHCP or fix address on the Ethernet when I start.
Is it possible to use HWI and lwiplib. or I need NDK only for TI RTOS?
Have you got an example on NDK to select fix address or dhcp ?
Thanks in advance
Christophe GG